Part Number: LMK04816
Tool/software:
Hi,
We have a board using the LMK04816, and due to an error the chip was supplied with 5V instead of 3.3V. We have rectified the issue and will replace the chip itself but need to know if the digital outputs (pins 45-47) would have also tried to output at 5V. This would cause damage to other areas of the design that will need to be looked into. According to the datasheet, the high value on the digital output is VCC, but in this case, we are not confident on whether that value would have been 3.3V or 5V.
Thanks,
Devin