This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: SYNC function with different input frequencies

Part Number: LMX2594

Tool/software:

Hello.

I want to combine multiple PLLs. The conditions are as follows:

・The OSCin frequency of each PLL is different.

・The RFout frequency is the same for all PLLs.

・Therefore, the settings of the N-divider in each PLL are also different.

In this case, is it possible to align the phase of the RFout signal using the SYNC function?

Best regards,

Atsurou Sambayashi