Part Number: LMK04821
Other Parts Discussed in Thread: LMK04816, LMK04803, LMK04906, LMK04208, LMK04832
Tool/software:
Hello,
I have a question about synchronizing multiple boards, each with one ADC, one LMK04821, and one FPGA.
Here's what I want to do:
・The interface between the AD converter and FPGA is JESD204B.
・The SYSREF mode for LMK04821 is planned to be SYSREF Pulser.
・The reference clock and synchronization signal are distributed to each board in phase using each LMK04821.
・The synchronization signal should be supplied to the SYNC/SYSRE_REQ pin or CLKin0 pin of each LMK04821.
・We would like to use this synchronization signal to simultaneously generate a SYSREF signal from the SDCLKout pin of each LMK04821 to synchronize the AD conversion of each board.
Question 1
Are there any problems with synchronizing using the above method?
Question 2
I cannot find any specification in the data sheet for the input timing of the synchronous signal supplied to the SYNC/SYSRE_REQ pin or CLKin0 pin.
How should I consider the setup time/hold time and the length of the synchronous signal to be supplied?
Question 3
If a synchronization signal is applied to the SYNC/SYSRE_REQ pin or CLKin0 pin of the LMK04821 on each board at the same time, can a SYSREF signal be generated from the SDCLKout pin of the LMK04821 on each board at the same time?
In that case, how should we consider the timing from the synchronization signal to the generation of the SYSREF signal?
Thank you,
Takayuki