Tool/software:
Do you recommend LMK1C family to fanout an arbitrary digital signal? Like a 3.3V SPI SDO or CS signal. Different duty cycles at different times, often DC.
I see there'd be an issue with enable / disable, but I figure there's a workaround.
Let's imagine 1G is always high. Then the LMK1C chip is enabled with 5 cycles on the CLKIN pin, then CLKIN does SPI CS behavior. And is never disabled. Would this work as I expect?