This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04101: Clk input termination resistor

Part Number: LMK04101

Tool/software:

Hi TI team,

We are using LMk04101 in one of our design and the reference clock input for the IC is fed from an single ended external source which is matched to 50ohms. Do we still require a 50ohms to ground at the input of CLKIN before the AC coupling capacitor for LMK04101?

What is the best way to interface the 50ohm matched clock source to the LMK04101?

(Note: U8 is LMK04101)

Regards,

Ratan