This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1104: Maximum Input Consumption Current

Part Number: LMK1C1104

Tool/software:

Hi everybody,

I would like to know the maximum input consumption current of this particular part, working with VDD = 3.3 V and all outputs active, 50Ohm load, 10 MHz frequency.

This parameter is usually labeled as "Total current into VDD" in other parts' datasheets.

Datasheet talks about "Core supply current" which at first I thought would be the answer to my question, but it refers a maximum of 40mA, when each output delivers 20mA.

Thanks for your help.

Regards,

  • PAB,

    The picture below contains the core supply current used by the entire device. At 3.3V the device burns a total of ~33mA. If that's not what you're looking for, what do you mean by input consumption current? How much current was burned by the input driver alone? What is this for?

    Best,

    Andrea

  • Hi Andrea!

    Thanks for your reply.

    In case every output (four outputs in the case of the LMK1C1104) is loaded with 50Ohm||5pF, what would be the core supply current of the device?

    Regards,

    PAB

  • PAB,

    Unfortunately we do not have data with a 50Ω load; however, because the data we have is across a 5pF load, I would assume the consumption across an added 50Ω would be the same since the capacitor alone acts like an open circuit. Adding the resistor in parallel would generate the same amount of current, the current would just dissipate across the resistor.

    Best,

    Andrea

  • Andrea, I got confused. How is it possible for this device to deliver 20mA per output (20ma x 4 outputs = 80mA), and just taking 33mA  from the supply?

  • PAB,

    The device is NOT taking 33mA per output, the ENTIRE device (so the core, the outputs, inputs, internal circuitry, etc) will all consume 33mA. With a 5pF load each output is consuming on average ~6.3mA.

    Best,

    Andrea

  • Andrea, I didn't say it is taking 33mA per output.

    I understand the whole device, with all its outputs active, will consume (maximum) 33mA (40mA). That's clear.

    Now, each output, with a 50Ohm||5pF load, is able to deliver approximately 20mA. That sums up 80mA. (I asked about this in this forum).

    How is it possible, for this device, to drive 80mA when there is a maximum current through VCC or GND through the entire device of 40mA? 

  • For those who this may be useful.

    I had to find the answer for myself.

    When they told me each output is able to drive up to 20mA, they didn’t mention not at the same time.

    Putting all outputs in parallel, with 50 Ohm load, it drives around 28,5mA, which perfectly correlates with those 33mA specified as typical core supply current on the datashet.

    Hope it helps.

    Regards.