Part Number: SE555
Tool/software:
Hello Everyone,
I'm trying to make a PWM signal for my MOSFET that is driving a heater.
I'm using the "Pulse Width Modulation Control" topology from electronics tutorial.
I designed the PCB and assembled all the components. For my application I wanted a 100mHz signal and based on my potentiometer size, I calculated and simulated (in LTSpice) that the discharging capacitor should be 22u.
Now if I use a 2220 packaging capacitor of 22u 50V 20% and X7R dielec, I'll get the same results as the one I anticipated and simulated. But when I'm using a 0603 packaging capacitor of 22u 25V 20% and X5R dielec, my frequency gets to 300mHz.
I triple checked my circuit and it's components, and all the values I soldered are 100% correct (I desoldered, measured the vale and then resoldered again) but I don't know the reason for the increase in frequency. Only the capacitor is changing and everything else is the unchanged.
Can it be because of ESL? but my frequency is not high though, so it shouldn't matter!