Part Number: LMC555
Tool/software:
Hallo TI,
I would like to get information about the input structures of LMC555. I read on forums that it has some input clamp diodes, but the datasheet does not mention it, no input clamp limit in "absolute maximum ratings". (By the way the GND-0.3V ÷ VCC+0.3V rating for inputs is suspicious.)
The origin of the question is this circuit. The input is AC-coupled to TRIGGER#. When the input is LOW for long C3 will charge to VCC, then a LOW->HIGH transition will rise the voltage on TRIGGER# to around 2*VCC, which is not good. But if the IC input has internal clamp diode to VCC, we don't need to add an external diode.

Thank you in advance.