Part Number: LMX1204
Tool/software:
LMX1204 output LOGICLKOUT(logic clock) failure issue.
Below is my design. Pin 2/3 is float. I want to output the LOGICLKOUT on pin 27/28. After I configure the LOGIC_EN (R8 register) and LOGICLKOUT_EN(R8 register), and USE DIVIDER(R9 register)). With PRE-DIV and DIVIDER all set to 4-4. The clock input is 1GHz, but no output signal from LOGICLKOUT on pin 27/28.
What is the problem? Could you help me.
Besides, I also use the LMX1204-EVM board to configure the LOGICLKOUT clock which is the same as my design, again no signa output.