This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: Power Down Function

Part Number: LMK04832

Tool/software:

Question on Power Down function.  If I was normal mode and then I assert power down function thru Register 0x002.  How do I bring up the chip back from Power down mode?  Do I need to follow a power up procedure where I need to issue a reset and then reprogram the device again? or should is just a matter of removing from power down mode?

  • You can just clear the POWERDOWN bit over the SPI bus. The SPI functions remain active even during POWERDOWN state, and register values are still retained (and can be modified) during the POWERDOWN state. Some triggered actions like PLL calibration, SYSREF pulser output, or dynamic digital delay triggers are not initiated when the triggering register is written during POWERDOWN state. The RESET trigger can still be initiated in POWERDOWN state, which also clears the POWERDOWN condition.

    POWERDOWN state also disables the PLLs. If you have outputs that need to be aligned, or input-to-output phase relationships in zero-delay mode that need to be preserved, note that exiting the POWERDOWN state is functionally equivalent to randomizing those phase alignments just like you would normally see after a POR sequence, and you would want to re-synchronize the device following whatever sync procedure you typically follow after POR.

  • Ok. Thank you Derek.