Part Number: LMX1204
Tool/software:
Hi,
Few questions:
- Assuming sysref_req pin is continuous. When I look on the Flowchart for SYSREF Windowing Operation, after toggling SYSREFREQ_CLR (0 -> 1 -> 0), will the measure will occur on once (on sysref_req pin rising edge) or will it occur repeatedly?
- for another use I think to do with the LMX1204, I would like to hear your opinion, Assuming I want to measure and correct timing between 2 clocks, a fast clk Vs slow clock, for example 2GHz & 10MHz.
- Can I connect the 10MHz signal to the sysref_req pin (as if it was a sysref)?
- will I successfully measure the timing, and distribute the shifted 10MHz clock on the sysref_out pins?
- Assuming I will work in sysref repeater mode, I saw that sysref_req is reclocked with clock output, do you thinks that the sysref_out pins will have reliable 10MHz clock? (As I said it’s not really a sysref)
BR,
Barak