Part Number: LMX2594
Other Parts Discussed in Thread: LMK04832, LMX2572
Tool/software:
There are 2 or 3 LMX2594 on the board. Their OSCin (100MHz) and SYNC (2.5MHz) are all from LMK04832, which are well aligned (LKM04832 are synchronized).
I like to get all LMX2594 outputs at either at 312.5MHz or 5GHz with VCO = 10GHz by using SYNC pin to get phase aligned (SYNCed) of all outputs.
I tried to enable the VCO_PHASE_SYNC = '1' as stated in the datasheet for 312.5MHZ outputs. However the PreR has to be 2 so that Fpd = 50MHz. See below left.
However I like to have higher Fpd, such as 100MHz or 200MHz (by enabling doubler), the TISC shows error on the N divider.
Any suggestions? Thank you.