This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: multi-device SYNC

Part Number: LMX2594
Other Parts Discussed in Thread: LMK04832

Tool/software:

There are LMX2594 and a LMK04832 on our board.

LMX2594 OSCIN and SYNC are all from LMK04832. Where OSCIN = 100MHz and SYNC = 2.5MHz. 

The OSCIN and SYNC traces are well matched from LMK04832 to LMX2594. 

The LMK04832 outputs are all aligned or synchronized between multi-boards. 

We need to get all LMX2594 outputs aligned or synchronized between multi-boards

1. Can SYNC be continuous signal? 

2. Was SYNC pin really needed here? 

I could not get LMX2594 in SYNC. The outputs are jittering when enable VCO_PHASE_SYNC. 

I'm looking for helps.