Part Number: LMK1C1102
Tool/software:
Hello Forum,
in the datasheet it is stated:
Supply voltage: 3.3 V, 2.5 V, or 1.8 V – 3.3-V tolerant input at all supply voltages
I want to use 1.8V supply, but 3.3V input clocks.
What happens with the jitter specification at this scenario? I haven't found something in the datasheet.
Can I still rely on the Jitter specs for VCC_1.8V or will that change with 3.3V inputs?
Thanks in advance!
BR Julian