This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Muti-board LMK clock

Part Number: LMK04828

Tool/software:

Hi experts,

I still have some questions about synchronizing multiple LMK devices. When I tested the 500MHz output from the LMKs on two clock boards, I noticed some jitter between on them, which also affected the LMX output.

My current configuration is based on the 2b case (dual loop nested ZDM) as shown in the diagram. I think that with ZDM, the 500MHz edge output should align with the edges of the 5MHz input. If both 5MHz edges are aligned, then both 500MHz edges should be aligned. I am currently using clkin0 as the 5MHz reference input, so do I still need to send a sync pulse to the sync pin to reset the divider? Could you point me in the right direction?

Thank you!

LMK04828 CLOCK FILE: 

MTS_5M_AutoRef_5M_SYSREF_250M_Clocks_0Delay_Nested_SYNC_new.tcs

Refer: https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1361403/lmk04828-multi-board-rfsoc/5205499?tisearch=e2e-sitesearch&keymatch=RFSOC#5205499

Regards,

Jingda