This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Problems were encountered in configuring clock output using TICS PRO software

Part Number: LMK04828

Tool/software:

At present, we want to use a piece of LMK04828 as the master clock,7 channels of DCLK output 0-2Ghz,7 channels of SDCLK output 10-20Mhz. The clock input of the chip Cin0 is 10M, Cin1 is 10M, Cin2 is 156.25M, OSCin is 100M, Cin0 and Cin2 are not connected at present. Using TICS_pro to configure the LVDS output of the full channel, but not all the channels can output the configured waveform. The 10M of SDCLK of the 7 channels seems to have no output. I hope you can help me see where there is a mistake in the configuration, or could you provide me with a configuration file of 2G plus 10Mhz for testing? Thank you very much! (Below is the schematic diagram of lmk04828 and the configuration file of TICS_pro I am currently using)

lmk04828_M.pdf                                                216_lmk04828cin0_10M_cin1_10M_osc100M.tcs