This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK1C1102: Request for selection of LVCMOS Clock buffer

Part Number: LMK1C1102

Tool/software:

Please consider my request and provide recommendations for a clock buffer that meets the following criteria:
  • Frequency Support: 52 MHz or higher
  • Voltage Compatibility: LVCMOS 1.2V for both input and output, with 3.3V tolerance if possible
  • Zero Delay: Must provide zero delay functionality
  • Phase Jitter: Should exhibit low additive phase jitter, preferably less than 250 fs

Your assistance in finding a suitable clock buffer that satisfies these requirements would be greatly appreciated.