Part Number: LMX2492-Q1
Other Parts Discussed in Thread: LMX2492
Tool/software:
I am also using the LMX2492 for an FMCW radar and have found that undesirable spurs that are created from using the chirp feature.
Like the previous designer, I am also seeing spurs that are ~11dBc that create a haystack effect:
Before reaching out, I have check my clock and power supplies as potential sources of the spurs, but now that I have seen this issue in another thread, I am convinced that this is primarily a chirp function behavior.
I am using a very clean, low phase noise 100MHz reference and have very clean < -80dB power supply noise.
Are there settings, that can be configured to minimize the fractional N spurs created while using the chirp feature or a set of recommended chirp pulse width/duration/frequency range for optimal performance?
Kind Regards,
Matthew