Part Number: LMKDB1202
Tool/software:
Hi, TI
I have a question regarding the LOS# operation of the LMKDB1202.
There are two clock inputs, but only one LOS# signal.
In this case, which clock input does the LOS# operate based on, CLKIN0 or CLKIN1?
When CLKIN_SEL_tri is set to Low (Default), it states that CLKIN0 becomes the source. Does this mean that the source that the LOS# operates on changes depending on the state of CLKIN_SEL_tri?
Additionally, if CLKIN0(CLKIN_SEL_tri is set to Low) is being used as the source, can the LOS# signal be used to check if CLKIN1 is receiving input correctly?
Thank you.