Tool/software:
Dear TI's engineers
We use the LMX2595EVM to generate a chirp signal with a central frequency of 13GHz and a swept bandwidth of 500MHz by the automatic mode of the evaluation board. However, I don't know why there always is a point-frequency signal at 12.87GHz. When I change the central frequency to 14GHz, the point-frequency signal still exists, and its location is at about 13.87GHz. Would you have any idea about the problem? Thanks a lot.
Best regards,
Jieru