Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: PLL1(CLKIN0) fails to Lock in DC Couple CMOS but locks in AC Coupling mode Bipolar

Part Number: LMK04832

Tool/software:

Hi

We are  using LMK04832 in design, 

CLKIN0 - 10MHz (OCXO), DC Coupled Input as shown in below circuit, 

PLL1 Led doesn't come up, assuming PLL1 fails to Lock, But PLL2  

OSCIN- 100MHz VCXO (Differential)

DC Coupled CLKINx

Attaching the LMK TICS file for reference

Another board with AC Coupled CLKINx is able lock & we could see lock led of PLL1

AC Coupled CLKINx

Please suggest.

Attached DC Coupled config file

HexRegisterValuesLMKCPOUTMAX_DRIVESTRENGTH.txt
R0 (INIT)	0x000090
R0	0x000010
R2	0x000200
R3	0x000306
R4	0x0004D1
R5	0x000563
R6	0x000670
R12	0x000C51
R13	0x000D04
R256	0x010010
R257	0x01010A
R258	0x010260
R259	0x010345
R260	0x010420
R261	0x010500
R262	0x010601
R263	0x010735
R264	0x010810
R265	0x01090A
R266	0x010A60
R267	0x010B45
R268	0x010C20
R269	0x010D00
R270	0x010E01
R271	0x010F11
R272	0x011010
R273	0x01110A
R274	0x011270
R275	0x011345
R276	0x011400
R277	0x011500
R278	0x011601
R279	0x011755
R280	0x011810
R281	0x01190A
R282	0x011A60
R283	0x011B45
R284	0x011C20
R285	0x011D00
R286	0x011E01
R287	0x011F53
R288	0x012010
R289	0x01210A
R290	0x012270
R291	0x012345
R292	0x012420
R293	0x012500
R294	0x012601
R295	0x012711
R296	0x012810
R297	0x01290A
R298	0x012A10
R299	0x012B45
R300	0x012C20
R301	0x012D00
R302	0x012E01
R303	0x012F41
R304	0x013010
R305	0x01310A
R306	0x013260
R307	0x013345
R308	0x013400
R309	0x013500
R310	0x013601
R311	0x013735
R312	0x013825
R313	0x013903
R314	0x013A02
R315	0x013B80
R316	0x013C00
R317	0x013D08
R318	0x013E03
R319	0x013F2D
R320	0x01400B
R321	0x014100
R322	0x014200
R323	0x014311
R324	0x0144FF
R325	0x014500
R326	0x014608
R327	0x01474E
R328	0x014802
R329	0x014942
R330	0x014A03
R331	0x014B06
R332	0x014C00
R333	0x014D00
R334	0x014EC0
R335	0x014F7F
R336	0x015001
R337	0x015102
R338	0x015200
R339	0x015300
R340	0x015402
R341	0x015500
R342	0x01560A
R343	0x015700
R344	0x01580A
R345	0x015900
R346	0x015A01
R347	0x015BDE
R348	0x015C20
R349	0x015D00
R350	0x015E1E
R351	0x015F0B
R352	0x016000
R353	0x016114
R354	0x016244
R355	0x016300
R356	0x016401
R357	0x016540
R361	0x016958
R362	0x016A20
R363	0x016B00
R364	0x016C00
R365	0x016D00
R366	0x016E13
R371	0x017310
R375	0x017700
R386	0x018200
R387	0x018300
R358	0x016600
R359	0x016700
R360	0x016801
R1365	0x055500