Other Parts Discussed in Thread: LMK04832EVM, , AFE7950EVM, LMX1204, USB2ANY
Tool/software:
Hi,
we've a complex setup with multiple AFE7950EVM, LMK04832EVM, LMX2694EP EVM and LMX1204EVM which need to be controlled from an AMD ZCU102 EvalBoard.
The LMX1204EVM has a built-in USB2ANY circuit, which is directly connected to the SPI channel of the LMX1204. No jumpers to disconnect the MCU from the LMX1204.
There is a SDK for the USB2ANY for Windows, but we need access from Linux (embedded on AMD ZCU102) to the LMX1204.
We need either
1) access to USB2ANY from Linux (preferred)
or
2) a way to inject external SPI signals without back powering the MCU (through R16, ...) => custom firmware with High-Z SPI
Regards,
Sebastian