Part Number: LMX2694-EP
Other Parts Discussed in Thread: LMX2594
Tool/software:
Hello,
I am using the LMX2694 to clock two identical devices using both differential outputs RFOUTA and RFOUTB. During my testing I noticed that I measure two vastly different voltages at each of the two outputs, with a difference of up to 50%. The output power difference is heavily dependent on the output frequency, especially for values between 4-8GHz.
As a method of verification I used the Evalboard containing the LMX2694 and I get similar results there, although they are not as bad as in my own design. Worst case I measured a difference in the output amplitude of 25%, independent on the output power or output MUX settings.
I am wondering whether this behaviour is expected or if both outputs should behave nearly identical regarding their output power? Is there any data available regarding the output power across frequency for each output and are similar values expected for all devices? In the datasheet of the LMX2594 is a graph available for a single ended output (Fig. 18), but there is no mention if the same value is expected for all output signals.
Kind regards,
Thomas