Part Number: LMK04828
Tool/software:

I am using two clock inputs from lmk04828.
1. 10MHz input from external balun at pins 34/35
2. VCTCXO 10MHz
(OSCIN)
The signal input to CLKin1 is used as a synchronization signal standard.
Is there a register or method that can readback when there is no input from CLKin1 / when input from CLKin1 comes in and is used as a synchronization signal?
Rather than measuring, we need a way to indicate that synchronization is set by inputting CLKin1 through a register.