Other Parts Discussed in Thread: CDCLVP111
Tool/software:
On the CDCLVP111 SP, can you confirm the output and internal current supply current is 405mA with all outputs (10) terminated to 50 Ohm ?
This current value takes into account load + CDCLVP111 ?
And the maximum internal current consumption with all (10) channels loaded of the CDCLVP111 is 85mA ?
For information in my case with only 3 loaded outputs I had measured 75mA (by remove the current of loads )
If this is the case, the component will dissipate 323mW (3.8*85mA) in a max in a WC scenario.
Thanks,