Part Number: LMX2572
Other Parts Discussed in Thread: LMX2594, LMX2595
Tool/software:
The synthesizer chip behaves normally with good spectrum and phase noise but when using the divider the spectrum is very poor and broad. However, when I use a foam tipped swab with cool spay, the divided spectrum is normal. I've tried reflowing the chip with no improvement.
I've successfully used the LMX2594 and LMX2595 with similar layout with no problems.
Shown below is the 5000MHz VCO output

Show below is the same synthesizer with the divide by 4 selected.

reg 0 = 0x209c (default=0x209d)
reg 5 = 0x20c8 (default=0x20c8)
reg 10 = 0x13f8 (default=0x1378)
reg 14 = 0x1840 (default=0x1840)
reg 29 = 0x0000 (default=0x0000)
reg 30 = 0x18a6 (default=0x18a6)
reg 36 = 0x0047 (default=0x0028)
reg 37 = 0x0205 (default=0x0205)
reg 38 = 0x0000 (default=0xffff)
reg 39 = 0x0007 (default=0xffff)
reg 42 = 0x0000 (default=0x0000)
reg 43 = 0x0003 (default=0x0000)
reg 44 = 0x22a2 (default=0x22a2)
reg 45 = 0xc600 (default=0xc600)
reg 46 = 0x07f3 (default=0x07f3)
reg 52 = 0x0421 (default=0x0421)
reg 57 = 0x0020 (default=0x0020)
reg 71 = 0x0080 (default=0x0080)
reg 75 = 0x0840 (default=0x0800)
reg 78 = 0x0065 (default=0x0065)
F(MHz) = 1250.0 = 5000.0 / 4 = 70 * (71 + 3 / 7) / 4 CP=8 PWR=34