This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2582: Pins 30, 40 and series SPI resistors

Part Number: LMX2582
Other Parts Discussed in Thread: ADC12DL3200EVM,

Tool/software:

Hi,

1) In ADC12DL3200EVM, PLL's pin 30 is connected to GND using 680 ohm PD resistor. In the datasheet, this pin is given as NC.

Can we keep LMX2582's pin 30 as NC?

2) In the same EVM, pin40 is tied to GND. Should the pin be tied to GND or kept as NC?

3) In the same EVM, 100-ohm series resistors are used in PLL's SPI bus. Are they required to be added? 

4) Can you please confirm how much current is to be expected on these PLL SPI pins?

Thanks