Tool/software:
On a Xilinx clk104 board, the J11 connected to LMK04828 pin 37 (CLK_IN0_P) via a 3 dB attenuator circuit below. 
J10 is connected to LMK04828 pin 56 SDCLK_OUT11_P though the attenuator below:

Typically, connect 0 dBm to the input J11, and measure the output from J10.
I connected the 0 dBm 10MHz signal to the J10 by mistake, and the board does not seem to be behaving correctly.
I want to know if this mistake can damage the LMK04828?
On datasheet, absolute maximum rating, only the differential input current is specified for +/- 5mA.
No specification on the input to the CLKoutX/X*.
Thanks