Other Parts Discussed in Thread: LMR70503
Tool/software:
Hi,
LM2662M has reached EOL and we have replaced it with LM2660MX. However, the LM266x lineup is a bit of a legacy product, so from the perspective of supply, we would like to consider a new product group for future new designs. Could you recommend a product with the following specifications?
- Input voltage: +2.5V
- Output voltage: -2.5V
- Output current: 0.2A
- Switching frequency: Approximately 150kHz
TPS63700 and LMR70503 are considered as replacement candidates, but it has been quite a while since these products were released. Since we place importance on long-term supply, we would prefer a new 300mm factory production or a product as new as possible.
Thanks,
Conor