Part Number: CDCLVD1208
Tool/software:
For unused clock input pins, a pull-down with 1KΩ is recommended, but is it not acceptable to connect them directly to GND?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCLVD1208
Tool/software:
For unused clock input pins, a pull-down with 1KΩ is recommended, but is it not acceptable to connect them directly to GND?
Hi Ikemoto-san,
You can leave floating due to built-in hysteresis or tied to GND via 1k PD. Both are acceptable.
Best regards,
Vicente
Thank you for your reply.
Is it acceptable to use 0Ω instead of 1kΩ for the pull-down?
Short the input to GND.
Best regards.
Hi Ikemoto-san,
Are you connecting an entire bank to GND (both the p and n inputs)? Or are you simply one n or one p to GND?
Thanks,
Michael
Ikemoto-san,
In that case, it might not be a bad idea to use a capacitor (i.e 0.1 microFarad) to connect the inputs to GND, but you can use a 0 Ω resistor.
Thanks,
Michael