Part Number: LMK04826
Other Parts Discussed in Thread: ADS52J90,
Tool/software:
I have trouble to snychronize two ADS52j90 with the LMK04826. I have 10 % of the startups a data mismatch by one clock cycle. Now I tried to startup the lmk as described in chapter "9.3.2.1.1 Setup of SYSREF Example" and "9.5.1 Recommended Programming Sequence".
In the chapter 9.5.1 there is the point "6. Program registers 0x166 to 0x1FFF" I don't understand.
Why is there a 16 Bit number instead of 8 Bit like the register size?
Do I have to do it even when I'm not using the PLL2?
And does it has to be the last command in the programming sequence?