Tool/software:
Hi:
We are using LMX2820 to generate 13-20GHz signal, In some frequency bands, the chip may lose lock if the same parameter( 2_b Change frequency operation as described below)is configured multiple times.
For example, if you configure 20G continuously for 500 times (each time with an interval of 20ms),
the chip will lose lock around the 300th time; other frequencies such as 18.9G will not lose lock.
What could be the reason? Thanks!
The details of the chip are roughly as follows:
1. The chip configuration is as shown in the figure:
2. Register Configuration method:
a.)Initialization
As 8.3 Initialization and Power-on Sequencing in LMX2820 datasheet.
b.)Change frequency operation
Thanks!