This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571EVM: PLL can not be locked

Part Number: LMX2571EVM
Other Parts Discussed in Thread: LMX2571

Tool/software:

Hi Expert

1.TICS PRO set up is as below, F_OSC_122.88M, F_IN_122.88M

2.Waveform of Fosc and Fin

F_IN

BRs

Peter Hsiao

  • Hi Peter,

    Did you program all registers? in the menu bar, click USB Communications --> Write All Registers.

    Check to see if the SPI communication is all right. Program below register will has noticeable current change.

    - Program POWERDOWN = 1

    - Set TX Enable, RX Enable = 1 or 0.

  • Hi Noel

    1.SPI communication is fine by test result as below

    Program POWERDOWN=1/0 CURR= 3.02mA /5.12mA

    OUTBUF_TX_EN_F1=1, OUTBUF_RX_EN_F1=1/0 CURR=5.12/4.39mA

    OUTBUF_RX_EN_F1=0, OUTBUF_TX_EN_F1=1/0 CURR=5.23/4.43mA

    2.Waveform of F_OSC, F_IN is as below


    3.At now TP_CPout_Ext=2.2V

    4.Remove F_OSC, 

    TP_CPout_Ext=1.98V

    5.PLL LED is still not shown locked

    BRs

    Peter Hsiao

  • Hi Peter,

    Is the F_osc single-ended or differential? Do you have external termination at OSCin? 

    set IPBUF_SE_DEFF_SEL according to your input format. If there is no external termination, enable IPBUFDIFF_TERM bit.

  • Hi Noel

    1."Is the F_osc single-ended or differential? Do you have external termination at OSCin?" [Peter] Yes, it is SE with a external termination.

    2.After removing components of  loop filter as below 1,2,3,4,5 , PLL is locked .

     

    3.What is the current should be provided by the 5V adapter? Is it 1A enough ?

    BRs

    Peter Hsiao

  • Hi Peter,

    Current consumption of the LMX2571 in PLL mode is about 10mA.