Part Number: LMC555
Other Parts Discussed in Thread: TPL5110-Q1, TPL5110
Tool/software:
Hi Experts,
I have attached the schematic and list of components:

I have not been able to do an actual test to see how much current it is drawing; it is very difficult. The circuit is integrated on a flex board that wraps around a 3v battery such as a cr2032. The components are very small, and the height of the chip components is max 1mm. so it can fit in a remove together with the battery. The battery and circuit go inside a remote control that is normally constantly transmitting. The purpose of the circuit is to shut the power from the battery to the remote when the remote is stationary for 8 seconds. Once the remote is picked up or any vibration the circuit will resume power to the remote. As long as the remote continues to be in motion the power for the remote will be active.
Let me know if you think I can somehow reduce the current to be in the teens. From the data sheet it shows 130uA current draw for the 555 timer; the battery is 220mAH. That would give approximately 60 days of battery use. If it was at 15uA, then the battery would last approximately 600 days which would be great.
I have 2 circuits that were in the remotes and after 2 months would not transmit because the battery is too low. It was a brand-new battery when I installed them.
For your assistance.
Regards,
Allan