This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMKDB1102: LMKDB1102

Part Number: LMKDB1102
Other Parts Discussed in Thread: CDCE6214

Tool/software:

I'm looking for a crystal based frequency translator to replace an old Vectron FX-500.  It had a 32MHz oscillator that was able to lock onto an 8MHz input clock.  It ran on 3.3V and had CMOS outputs.  Would you have anything close?
Thank you.
  • Hello George, 
    We don't have frequency translators with this exact topology but you can use a clock generator for example to take an 8MHz input and generate a 32MHz output. 
    A suitable device would be CDCE6214. 

    Is there a specific jitter requirement your application has over a certain integration band? 

    Best Regards, 

    Vicente