Part Number: LMX2820
Tool/software:
Hi,
As shown in the topology below, the LMX2820 works in Cat.3 synchronization mode.
Whether to support the phase alignment of the output clocks of two chips, the error phase between the two outputs is fixed.
There is no bimodal distribution like that described in the data sheet. Because the chip works in a network analyzer-like mode,
different LMX2820s are used for reception and transmission to generate LO, which is very sensitive to phase changes.
Thanks!