Part Number: LMX2572LP
Tool/software:
Hi,
The setting is as below.

spur is as below.

In the graph, Fout%Fosc is 12MHz offset. is it correct? not 26.4MHz?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2572LP
Tool/software:
Hi,
The setting is as below.

spur is as below.

In the graph, Fout%Fosc is 12MHz offset. is it correct? not 26.4MHz?
Thanks.
Yes, you are correct. This should be the distance to the closest integer boundary. We could claim that this 410.4 MHz is 26.4 MHz away from a multiple of 38.4 MHz, but it is also 12 MHz from an integer multiple. So it should choose the 12 MHz.
I'm updating the PLLatinum Sim to include oscillators, so I'll fix this, but likely this will go out in December.
Hi Dean,
Thanks for your answer.
In the graph, 12MHz is highest.
I confused if 12MHz spur is highest or 26.4MHz spur is highest.
Which is highest among Fout%Fosc and integer multiple?
Thanks.
Hi David,
The simulation predict 12Mhz spurs is -130dBm, which is super small. At 26.4MHz, it is expected that the level will be even smaller.
Actual measurement does not see any spurs at 26.4MHz offset.