Part Number: LMK00301
Tool/software:
Hi,
The datasheet feature says the LVDS frequency range is DC to 2100MHz, but the specification table says 1.0GHz to 1.6GHz, and Figure 7-2 shows the LVDS Output Swing (VOD) vs. Frequency range as 100MHz to 1.3GHz. So, which one is the correct frequency range?
Our output frequency range is 150MHz to 200MHz LVDS signaling at this frequency. Will it cause any problems?
We have bought your EVB and tested it with 150MHz to 200MHz LVDS output, and it works fine.