Tool/software:
Hi,
I would like to work with LMK1C1104 with sine wave at its input.
The sine wave will go thru 10nF capacitor and 100R pull up/down resistors into VDD=1.8V
The minimum level of the 100MHz sine wave is 0dBm ~ 0.63Vpp
For ease of calculation (and some design margin), lets discuss about minimum level of 0.6Vpp
At LMK1C1104 DS I can see that VIH is 0.7xVDD (1.26V) , VIL is 0.3xVDD (0.54V)
According to application note snaa411 it is written that the set point is Vt, but VIH, VIL are recommended

Does 0.6Vpp that will fluctuate from 1.2V to 0.6V (both not reach VIH, VIL) and swing around Vt=0.9V should work?
PS - I made lab measurements with signal as low as 400mVpp and still get good signal at the output side (with duty cycle of 47%) which is OK.
I'm not sure that I understand the VIH, VIL correctly (DS looks as mandatory, application note looks as a recommendation).
In addition, can you explain regarding the slew rate of the 100MHz as 0.6vpp (+0.3V to -0.3V) - I'm not sure how it should be calculation (and again), is it a solid requirement?
Below is the setup to check the Sine signal (as low as 400mVpp) with 1.8V VDD

Below is the 100MHz 1.8V CMOS output when input sine is 400mVpp

Thanks,
Zeev.