This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2615EVM-CVAL: Spurious Observed in Spectrum output

Part Number: LMX2615EVM-CVAL


Tool/software:

I using 10MHz input reference for LMX2615EVM-CVAL board. I am generated output frequency around 6.84 GHz and observed the output spectrum. While generating integer output (6.840 GHz), I observed band of spurious about 3.7KH ( and it's multiples) away from center frequency. Same were not seen in case of fractional output (6.8346 GHz), and small spurious was observed around 840 Hz.

What could be reason for spurious observed in case of integer output? Why same are not seen in case of fractional output? What are remedies available (in case of LMX2615) in order to obtain clean spectrum? 

I am attaching above spectrum output for your reference.

Kindly note, 10 MHz input reference itself had a clean spectrum and no such spurious were observed.

Regards

Deepak