Part Number: LMK00334
Tool/software:
Wondering if I can remove the blocking caps I have in place on the CLK0 inputs from the PCIe interface [gold finders in this case].
Also the downstream connections will have blocking caps in place - on those modules [XMCs]. I have 49.9 pull-downs in the circuit located at the LMK00334. Pretty standard and would expect to work but figured I would ask.
Last, I put in a filter -> 3.3V 10uF-600 ohm /.5 ohm - 1 uF to feed all of the pins with individual .1 uF at each pin. Figured a mini-plane under the device would be a good way to make this happen. Caps on the back, via at each of the 8 power pins. I saw in the diagrams on this one that there are separate circuits for each power type. Is that really necessary?