This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM: Is it possible to achieve 1 GHz bandwidth on a FMCW signal with the LMX2594 EVM evaluation board?

Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594, LMX2492

Tool/software:

I am doing a FMCW project and I would like to know if, to get a chirp at 10GHz and with a bandwidth of 1GHz, it is enough only with the LMX2594 EVM evaluation board or it is needed some additional component?