Part Number: LMX2572LP
Tool/software:
Thank you for your previous answer. I have some more:
1. Regarding your previous answer, do you think that combined the signals from both ports using short wires (A+ to B+, A- to B-) allows me to cheaply get extra 3dB power? (assuming I will find a way to properly route these nets). I think that this what you originally meant in your answer but I was not sure...
2. Do figures 17, 18, 155, 156 refer to a single ended output power or to a differential one?
3. According to RF OUTPUT specification, a single ended output power at 2GHz with OUTxPWR=15 is 5dBm.
According to to figure 18 (156) it seems that for 2GHz, with OUTx_PWR=15, the output power is 6dBm. Is it a typo in the datasheet?
Thanks,
Roy