Other Parts Discussed in Thread: LMK03328
Tool/software:
Hello,
I am planning on using the LMK03328 in our design. I have some questions relating to the jitter performance. Is jitter performance different if I use a 100 MHz reference clock vs a 50MHz crystal?
Also, do I have to use the SECREF input? Can I still use PLL2 with the SECREF input disabled? If so, what is the purpose of having this input?
Lastly, TICSPro says I can make this configuration work with a single PLL. I don't see how that is possible. See the image for my configuration.
Thanks,
Ryan