Part Number: CDCEL937-Q1
Other Parts Discussed in Thread: CDCE913
Tool/software:
Hi Ti team,
Im planning to use the CDCEL937QPWRQ1 clock buffer with Input oscillator of 27Mhz & 6 output clock as 27Mhz, the supply & output voltage of 1.8V. While doing DC analysis there are VOH, VOL values for multiple source & sink current. The receiver side 6x clock inputs source & sink current is not given in the datasheet. In that condition which VOH, VOL values to be considered or do we have any options to calculate the Source & sink currents.
6x clocks will be given to a sensor which has Vih=0.7*1.8=1.26V, VIL=0.3*1.8=0.54V
Please let me know.