This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04610: Clock & timing forum

Part Number: LMK04610
Other Parts Discussed in Thread: LMK04828, , LMK04832, LMX2572, LMK1D2104

Tool/software:

The answer record on the LMK04828: LMK04828 vs LMK04610 post states that the LMK04610, "skew across outputs can be around 100s of ps across PVT." but in the datasheet: |TSKEW| Maximum CLKoutX to CLKoutY has a MAX of 95ps. So which is it?? This part is very low power and desirable in my application, particularly due to the HSDS outputs instead of LVPECL (although the outputs are incorrectly listed as LVDS and LVPECL both on the Clock Jitter Cleaners search table webpage and the LMK04610 page itself). The post also makes it sound as though this part is not recommended for new designs due to other issues/bugs and limited support, however, its still listed as ACTIVE by TI...so which is it? Lastly, if this is a part that is still OK to use, what is the CORE Power when in Bypass PLL1 and PLL2 mode? I am mainly trying to use this as a passthrough buffer with SYSREF divide and phase delay capability. The application is battery powered so power is important and the ~1W of power of the LMK048XX devices is too great. 

  • Output to output skew on the same device has a max of 95ps. The variation in part-to-part skew, even for the same output, is 100s of ps across PVT. The propagation delay variation over temperature for a single output is also 100s of ps, but the output blocks are at roughly the same temperature during operation and have roughly the same propagation delay temperature coefficient, so they tend to skew together - nevertheless, the skew between outputs should not be treated as constant across temperature.

    The part is still active, we still support it, it just did a lot differently from most of our other PLLs and that makes it challenging to work with and to support. It was designed with a very specific use case in mind, and other use cases tend to encounter one or more unusual difficulties. The reason it can be so low power is because of a novel semi-digital PLL architecture, but that same architecture results in PLL1 wander even while locked, which is well-documented across the forum; other implementation choices like the use of a primarily-CMOS process instead of a BiCMOS process led to large propagation delay variation across temperature relative to our BiCMOS PLLs like LMK04828 or LMK04832, which can be surprising for people trying to use it in applications where skew and prop delay variation should be minimal; and there are several unexpected limitations, like the relationship between SYNC/SYSREF triggering and PLL2 PFD frequency, which are occasionally a nuisance - in this case, it would seem, a highly relevant nuisance.

    The SYNC and SYSREF triggers are re-timed by the output of the VCO post-divider. If you do not have the post-divider engaged (i.e. the VCO on), the SYNC and SYSREF cannot be activated. Additionally, there is a re-timer on the GLOBAL_SYNC and GLOBAL_SYSREF signals as well as the signals generated by the SYNC pin, which implies that PLL2 must be on (even if not locked) and a reference signal must be applied to PLL2, in order to use the SYNC or SYSREF behaviors. This device is not designed to function as a pure clock + SYSREF distribution passthrough buffer. If you really want to make LMK04610 work this way, using only the documented register set, you need to enable PLL2, lock it to synchronize the VCO post-divider with the clock distribution signal, and also route PLL2 CLKin to the output channels. If the SYSREF frequency exceeds the state machine clock divider frequency, the SYSREF will not trigger reliably; meanwhile, the state machine frequency is strictly a power-of-2 divider from the PLL2 reference clock (see PLL2_REF_DIGCLK_DIV field) with a maximum divide of 32 and a maximum frequency of 50MHz, meaning there are cases between 50MHz and 25MHz where the SYSREF cannot be reliably generated at all. Incidentally, the SYNC is also re-timed by the PLL2 reference clock-derived state machine clock and the VCO post-divider, so aligning the dividers initially also requires PLL2 to be enabled.

    I think there are some override bits in register 0x148 that can force an asynchronous SYNC and SYSREF trigger signal without all the retiming through PLL2 and the VCO post-divider - setting 0x147 to 0x0C and 0x148 to 0x03 should force a trigger to the SYNC and SYSREF of each enabled channel, respectively, but I haven't tested this, and it's not necessarily guaranteed to work since it isn't production tested (though if the method is correct, it's extremely unlikely to fail in practice, since it would take an incredibly specific defect). Assuming this works, you could at least generate asynchronous SPI triggers for both SYNC and SYSREF - it would be sufficient for a single-device use case where there's no timing-critical window for the SYNC or SYSREF to be generated. If this isn't good enough, i.e. if you have to deliver the SYNC or SYSREF signals at a specific moment, or if you have multiple LMK04610 devices to synchronize, you would have to temporarily enable and lock PLL2 at startup or whenever a SYSREF pulse must be generated.

    For power consumption, consult table 226 in the datasheet. Any block you don't have enabled can be treated as nearly-zero current consumption (<1mA).

  • If there is truly no CORE power in bypass mode that leaves the total power at 196mW for Five HSDS 8mA outputs with Two of those designated as SYSREF signals and the dividers turned on. As far as I know TI does not have any part with SYSREF capability that is close to that low of power. But at the same time, I do not want a bunch of potential issues that this part seems to have. I only need one IC so I do not care about device-to-device skew, only CLOCK + SYSREF pair skew. I need LVPECL voltage levels and jitter spec, but it doesn't have to be LVPECL, which is why I liked the low power of these HSDS outputs. But as far as I can see on the webpage this is the only part that uses them. What is the next lowest power device I could use to accomplish my goal?

  • The next lowest output power device with SYSREF capability is the LMK04832, which even for an optimal configuration will still be around 1W. An alternate two-device solution uses LMX2572 as a SYSREF generator and LMK1D2104 as a dual-path independent distribution buffer, which would only be around 0.5W, but it has several drawbacks (inserting a PLL where none is strictly needed; only up to 500mV swing on the outputs instead of requested LVPECL spec).

    If LMK04610 is too much of a headache, I think you may need to look elsewhere. But since it doesn't sound like you have any severe timing-critical concerns about SYNC and SYSREF pulse timing, just the clock to SYSREF skew requirement, I think it's worth at least trying LMK04610 if it offers that much of a power advantage over the alternatives. If you give me the desired frequency plan, I can test it on an evaluation module in our lab.

  • This image is what I am trying to accomplish. The first clock/SYSRE pair need to be aligned and the second set of two clocks and one SYSREF need to be aligned as indicated by the red circle. I also need two other 200MHz clocks and two 50MHz clocks by themselves which are not aligned with any other signal. 

  • Hello,

    The team is out for the holidays. Please expect a response by Jan 2 at the earliest.

    Thanks,

    Kadeem

  • Kevin,

    The team member is still out of office. My apologies for the delay. Please expect a response by Jan 6th.

    Thanks,

    Kadeem

  • I didn't get a chance to check this today, but it's the first thing on my list tomorrow; apologies and thanks for your patience...

  • I spent most of today testing this, and came to the conclusion that unless PLL2 is on, even with forces applied, it is not possible to trigger the SYSREF. Enabling the PLL does add about 100mA on the 3.3V rail, and it needs to stay on as long as a SYSREF needs to be generated (it cannot be disabled and re-enabled later to generate the SYSREF on-demand). So I don't think LMK04610 is a good fit for a distribution-mode application like this.

  • Do you mean there is no way to trigger SYSREF at will, or there is no way to ever get SYSREF to come up without PLL2? I may not need an at-will on/off SYSREF capability. If it comes on at programming time and stays on that would suffice (without PLL2 on). If this is the case, what is the next lowest power TI part you would suggest (LMX2572 as a SYSREF generator and LMK1D2104 does not seem like a good solution in our case).

  • I should have asked if continuous SYSREF was acceptable... Specifically, the SYSREF pulser cannot be triggered without PLL2 active. If you can use a continuous 1MHz clock with the appropriate phase alignment as a SYSREF, this is definitely doable, and you can even guarantee alignment between the 200MHz clocks and the 1MHz clock without the need for a SYNC signal by assigning the SYSREF to CLKOUT3/4 which shares a divider - all 200MHz signals will be in-phase by definition since they are in divide-by-1 mode and cannot be anything other than in-phase, and the SYSREFs would come from only one divider so their phase would be shared on both outputs.

    The TICS Pro configuration below demonstrates this capability, along with the other 200MHz and 50MHz clocks for which no alignment was specified. I've checked this configuration on an oscilloscope with matched cables for the 200MHz and 1MHz signals, and I see the expected alignment (see the oscilloscope plot below which checks alignment between 200MHz CLKOUT1 and 1MHz CLKOUT3). This setup is still attached to the machine which captured the plot, so if you have additional data you'd like to see (e.g. skew) let me know.

    If you have an EVM, you can test the configuration on a device:

    • Prepare the device with 3.3V to the core supplies which require it, 1.8V to other lower power supplies as needed, and 200MHz into CLKIN1
    • Load the configuration into TICS Pro
    • On the User Controls page, in the Pins divider, toggle the RESETN pin HIGH -> LOW -> HIGH to reset the device
    • Write all registers, using either the top toolbar button or by pressing Ctrl + L shortcut
    • On the "Generic" page in the page tree, click the "Device Start" button in the lower left of the page to write the startup bit. At this point, all clocks should come up, including the requested 200MHz and 1MHz phase-aligned clocks, with the 1MHz clocks aligned to the falling edge of the 200MHz clocks (this depends on the duty cycle of the 200MHz input - if the duty cycle is 50% it should come up on the falling edge, otherwise it may be off by as much as the input duty cycle variation from 50%)

    LMK04610_distribution_200MHz.tcs