This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM555: How to use LM555 with a passive transducers?

Part Number: LM555
Other Parts Discussed in Thread: NE555

Tool/software:

Hello friends, I am working on a project where I am only allowed to use analog components. I cannot use ICs, microcontrollers, or microprocessors. I plan to use a passive transducer pair as a motion sensor. The main component I need to use in my circuit is the 555 Timer. I will use the 555 Timer as a 40kHz wave generator to drive the transducers. A part of the circuit's schematic is shown in the image below. However, I am not sure how to connect the transducer pair. Could you help me with this?
(Also, this circuit is not mine. It’s a 555 Timer circuit I found online that outputs a 40kHz signal. How should I connect the transducers to the output of this circuit?)