Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

LMK3H0102EVM: LMK3H0102EVM

Part Number: LMK3H0102EVM
Other Parts Discussed in Thread: USB2ANY

Tool/software:

I recently purchased an LMK3H0102EVM board and installed the TICS Pro 2 software.  I intend to use 125MHz outputs with or without SSC DC coupled to OUT1p/n.  When I connect the EVM via USB on J19 I see LED D5 illuminate.  I verified the jumpers are all set to i2c mode.  However the software always reports i2c error.  

When I did a scan of the bus it does not see a device.  ------------------------------ 

I dont have a scope to verify he default 100M is coming out yet.

Any suggestions on why TICS Pro 2 doesn't see my EVM board?

Thanks,

Charley