Part Number: LMK1C1104
Other Parts Discussed in Thread: LMK01000, LMK04832, SN65LVELT23, LMX2820, LMX2594, DDS39RF10
Tool/software:
Hi,
I would like to generate single ended CMOS clocks (< 250 MHz) with 10%, 25%, 50% and 75% duty cycle on the board. The generated clocks will be fed to transmission lines (< 3" long). The transmission lines will serve as a test structure that will be "probed". The transmission line does not need to drive a receiver, although I may put in a buffer to drive the signal into an O-scope.
To generate the non-50% duty cycle, I was thinking of using CMOS gates after the clock buffer (like gated clocks in CMOS VLSI). Are there pre-built solutions to accomplish this? Can the SN74AHC family be used to accomplish what I have in mind?
What are my options for extending this functionality to ~650MHz - 1GHz? I know that I would need to move to something like LVPECL and not LVCMOS, but, I am in the dark, how to generate non-50% duty cycles in this regime.
Thanks in advance for any pointers.
Regards,
Prasoon