This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00804B-Q1: fanout for PWM signals in multi-line Lidar application

Part Number: LMK00804B-Q1


Tool/software:

HI BU team

My customer is developing the multi-line flash Lidar application. They need a pwm signals to fanout to the coming MOS drivers. 

The PWM waveform is shown in below screenshot. 

The pwm signals is 3.3V and need total 12 channel outputs. The pulse width is 5ns , the pwm frequencty is about 2MHz( duty cycle is 0.046%), trising=307ps (20%-80%),tfalling=287ps (20%-80%). 

Is LMK00804B-Q1 ok for this application? if not, what's your suggestion on new solution with automotive level?

Thanks